Select a DL-SCH channel in the Channel
Setup node, then click the
button in the Transmission
Configuration cell to open the DL-SCH Tx sequence window.
The DL-SCH TX window displays the transmission sequence defined in the Channel Setup node for the selected DL-SCH channel.
You can make adjustments to the MCS index, RV index, VRB type, VRB offset, VRB size, and scrambling for each DL-SCH transmission from within the DL-SCH Tx sequence window.
The settings configured in the Channel Setup node and the DL-SCH Tx sequence window are displayed in the Tx Map.
Use the Import tab to navigate to and import a saved transmission sequence.
Use the Export tab to save the current transmission sequence to a file.
Click the button
to access a drop-down list
that enables you to set parameters for all transmissions to the same value.
DL-SCH Tx sequence window (Shown with parameters that are displayed when the RNTI Type is set to C-RNTI.)
|
N_1A_PRB (for SI-RNTI or P-RNTI) |
Displays the sequential number.
Displays the radio frame number.
Displays the subframe number (0 to 9) in a radio frame.
Choice: On | Off
Double-click or use the drop-down menu to turn the subframe state on or off.
When this parameter is on, other settings on this subframe are visible. Otherwise they are invisible.
When the DL-SCH parameter RNTI = 65535 (SI-RNTI) case, default is “Off” and there is no restriction for transmittable subframe. Otherwise “On”.
Choice: Off | 0 | 1 | 2 | … | 31
Default: 0
Double-click or use the drop-down menu to select MCS index for the subframe.
DL-SCH parameter RNTI = 1 to 65523 (C-RNTI) case, this parameter is as follows:
Where MCS = 0 to 28, Mod, TBS and TB Size are automatically decided.
Where MCS = 29 to 31, Mod and TB Size are read only and set by the software, TBS is selectable.
Where DCI Format = 2 or 2A or 2B, and MCS = 0, and RV = 0, TB is disabled (key of no transmission).
Where MCS = Off, TBS and Mod are available to set manually.
DL-SCH parameter RNTI = 65535 (SI-RNTI) case, this parameter is as follows:
Where MCS = 0 to 26 and DCI Format 1C, ‘MCS’ = ‘TBS’ as read only parameter.
Where MCS = 0 to 28 and DCI Format 1A, ‘MCS’ = ‘TBS’ as read only parameter.
Where MCS = 29 to 31 and DCI Format 1A, ‘TBS’ is available to set manually.
Where MCS = Off, ‘TBS’ and ‘Mod’ are available to set by manual.
For more details, refer to 3GPP TS 36.213.
Choice: QPSK | 16QAM | 64QAM (Modulation and TBS Index Table 1)
QPSK | 16QAM | 64QAM | 256QAM ( Modulation and TBS Index Table 2)
Double-click or use the drop-down menu to select modulation type for the subframe.
DL-SCH parameter RNTI = 1 to 65523 (C-RNTI) case, this parameter is as follows:
Where MCS is 0 to 31, the modulation is read only and set by the software.
Where MCS is off,the modulation is available to set manually.
DL-SCH parameter RNTI = 65535 (SI-RNTI) case, this parameter is as follows:
Where MCS is 0 to 31, Mod = QPSK as a read only parameter.
Where MCS is off, Mod is available to set manually.
For more details, refer to 3GPP TS 36.213.
Choices: Off | 0| 1 | 2 | … | 26 (Modulation and TBS Index Table 1)
Off | 0| 1 | 2 | … | 33 (Modulation and TBS Index Table 2)
Double-click or use the drop-down menu to select TBS Index for the subframe.
DL-SCH parameter RNTI = 1 to 65523 (C-RNTI) case, this parameter is as follows.
Where MCS is 0 to 28 with table 1 or 0 to 29 with table 2, TBS is read only and set by the software
Where MCS is 29 to 31 with table 1 or 28 to 31 with table 2, TBS is available to set manually
DL-SCH parameter RNTI = 65535 (SI-RNTI) case, this parameter is as follows.
Where MCS = 0 to 31 and DCI Format 1C, MCS = TBS as a read only parameter.
Where MCS = 0 to 26 and DCI Format 1A, MCS = TBS as a read only parameter.
Where MCS = 29 to 31 and DCI Format 1A, TBS is available to set manually.
Where MCS = Off, TBS is available to set manually.
For more details, refer to 3GPP TS 36.213.
Range: 1 to 97896 (C-RNTI mapped to one layer) or limited by UE Category
1 to 195816 (C-RNTI mapped to two layers) or limited by UE Category
1 to 1293736 (C-RNTI, mapped to three layers) or limited by UE Category
1 to 391656 (C-RNTI, mapped to four layers) or limited by UE Category
1 to 2216 (SI-RNTI or P-RNTI)
The maximum range value is dependent on the UE Category and the number of spatial multiplexing layers mapped to the transport block.
Where TBS = Off, this parameter is available to change manually. Otherwise this is a read only parameter set (0 to 26) by the software.
Where MCS = 29 to 31, this case is an exception. TBS, TB Size, and Mod are available to change manually.
For more details, refer to 3GPP TS 36.213.
Choice: Off | On
Sets the re-transmission process of the transport block 1 (codeword 0) for the corresponding PDSCH transmission. (Toggle the new data indicator state or not.)
On: Re-transmission data with next RV index is transmitted. (The new data indicator is not toggled.)
Off: New data is transmitted. (The new data indicator is toggled.)
First transmission of each process is not available to set re-transmission.
For example, if the Number of HARQ Processes is 8 (Assigned Process is 0-7) and every subframe transmission is on, the re-transmission is not available to the eighth transmission from the first transmission.
This parameter appears only when UE Type is set to Non-BL/CE.
See 3GPP TS 36.212 and 36.213, for more information.
This parameter selects the number of physical resource blocks.
This parameter indicates RV Index for each subframe respectively.
Where DL-SCH parameter RNTI = 1 to 65523 (C-RNTI) and RV Index Configuration = Auto case, this parameter is automatically decided by both RV Index Sequence and ReTrans parameters.
Where DL-SCH parameter RNTI = 65535 (SI-RNTI), this parameter is set to manually.
For more details, refer to 3GPP TS 36.321.
Choice: Type 0 | Type 1 | Type 2
Default: Type 0
Double-click or use the drop-down menu to select the downlink resource allocation type.
Type 0: Allocation of Virtual Resource Blocks (VRBs) of localized type is defined by RBG Bitmap.
Type 1: Allocation of VRBs of localized type is defined by Subset, Shift and RBG Bitmap.
Type 2: Allocation of VRBs is defined by VRB Type, RB Offset and RB Size.
See 3GPP TS 36.213 7.1.6 for more information.
Range:
0 (System Bandwidth = 1.4 MHz)
0 to 1 (System Bandwidth = 3 MHz or 5 MHz)
0 to 2 (System Bandwidth = 10 MHz)
0 to 3 (System Bandwidth = 15 MHz or 20 MHz)
Default: 0
Enter Subset of DL-SCH.
The parameter is visible when all of the following conditions are met.
- DL-SCH State is On.
- RA Type is Type 1.
- Subframe State is On.
- ABS is Off or ABS is On and ABS Pattern info indicates 0 for the corresponding subframe.
Otherwise, this parameter is invisible and not applicable.
See 3GPP TS 36.213 7.1.6.2 for more information.
Choice: Off | On
Default: Off
Double-click or use the drop-down menu to turn Shift of DL-SCH on or off.
The parameter is visible when all of the following conditions are met.
- DL-SCH State is On.
- RA Type is Type 1.
- Subframe State is On.
- ABS is Off or ABS is On and ABS Pattern info indicates 0 for the corresponding subframe.
Otherwise, this parameter is invisible and not applicable.
See 3GPP TS 36.213 7.1.6.2 for more information.
Length:
6 (System Bandwidth = 1.4 MHz and RA Type = Type 0 or System Bandwidth = 3 MHz and RA Type = Type 1)
8 (System Bandwidth = 3 MHz and RA Type = Type 0)
11 (System Bandwidth = 5 MHz and RA Type = Type 1)
13 (System Bandwidth = 5 MHz and RA Type = Type 0)
14 (System Bandwidth = 10 MHz and RA Type = Type 1)
16 (System Bandwidth = 15 MHz and RA Type = Type 1)
17 (System Bandwidth = 10 MHz and RA Type = Type 0)
19 (System Bandwidth = 15 MHz and RA Type = Type 0)
22 (System Bandwidth = 20 MHz and RA Type = Type 1)
25 (System Bandwidth = 20 MHz and RA Type = Type 0)
Default: 17 (all “1”)
Use the Bitmap Edit dialog box to set RBG Bitmap of DL-SCH.
Value 0 indicates that corresponding RBG is allocated.
Value 1 indicates that corresponding RBG is not allocated.
The parameter is visible when all of the following conditions are met.
- DL-SCH State is On.
- RA Type is other than Type 2.
- Subframe State is On
- ABS is Off or ABS is On and ABS Pattern info indicates 0 for the corresponding subframe.
Otherwise, this parameter is invisible and not applicable.
See 3GPP TS 36.213 7.1.6.1 and 7.1.6.2 for more information.
When System Bandwidth is less than or equal to 10 PRBs, Resource Allocation Type is automatically set to Type 0.
Choice: Localized | Distributed
Default: Localized
Double-click or use the drop-down menu to select the virtual resource block type for the subframe.
Where DL-SCH parameter RNTI = 1 to 65523 (C-RNTI) and RA Type = Type2 case, this parameter is available to select Localized or Distributed.
Where DL-SCH parameter RNTI = 65535 (SI-RNTI), this parameter is as follows:
Localized, corresponding DCI is only available Format 1A.
‘Distributed, corresponding DCI is available Format 1A or 1C.
For more details, refer to 3GPP TS 36.211 and 36.213.
Range: Depends on relative parameters as follows:
0 to System BW RB size – 1 (RNTI = 1 to 65523 (C-RNTI) case)
0 to System BW RB size - RB Size (Format 1A, Localized)
0 to System BW RB size - N_DL_VRB (Format 1A, Distributed)
0 to System BW RB size - N_step_RB to Floor(N_DL_VRB / N_step_RB)*N_step_RB (Format 1C, Distributed)
Enter the RB offset for the subframe.
For more details, refer to 3GPP TS 36.213.
Range: Depends on relative parameters as follows.
1 to System BW RB size (Format 1A, Localized)
1 to N_DL_VRB (Format 1A, Distributed)
N_step_RB to Floor(N_DL_VRB/N_step_RB)*N_step_RB (Format 1C, Distributed)
Enter the RB size for the subframe.
When the System Bandwidth is decreased, the DL-SCH Tx Sequence window's RB size, and some of the other data channel's settings, are reconfigured, similar to when a Predefined Configuration is executed. But, when the System Bandwidth is increased, no change to the DL-SCH Tx Sequence window's RB size, or the other data channel's settings occurs.
For more details, refer to 3GPP TS 36.213.
Choice: Ngap, 1 | Ngap, 2
Double-click or use the drop-down menu to select the RB Gap for the subframe.
Only VRB Type = ‘Distributed’ case this parameter is visible.
VRB Type = Distributed and System BW >= 50 case, this parameter is selectable by manual.
VRB Type = Distributed and System BW < 50 case, this parameter is read only and Ngap, 1.
For more details, refer to 3GPP TS 36.213.
Range: 0–3
Default: 0
Coupling: Visible when the Transmission Mode selection is 10.
Enter a value for the PDSCH RE Mapping and Quasi-Co-Location Indicator.
See 3GPP TS 36.211, 36.212, 36.213 and 36.331 for more information.